2018-11-26 11:49 PM
Hello,
I have to use STM32F030C6 controller. it has only one SPI interface.
in my project i want to connect external flash memory and TFT DISPLAY both on single SPI with controller.
problem is TFT display is 3-wire SPI interface & flash memory is 4-wire SPI interface.
in 3-wire SPI generally MOSI pin is connected to MISO through 10K resistor.
So how to i configure single SPI of controller as both 3 and 4-wire SPI interface.
Thank you
2018-11-26 11:55 PM
Options may be
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.