2024-05-21 8:01 PM - edited 2024-05-21 8:02 PM
I now need to update the CCR1~CCR3 register at the same time with DMA with DMAR register, I use STM32F103C8T6, I use STM32F10x_StdPeriph_Lib_V3.6.0\Project\STM32F10x_StdPeriph_Examples\TIM\DMABurst example, in the example DMA is Normal mode, I need to keep updating the CCRx registers, so I changed the DMA to Circular mode, but the CCRx registers are not updated as I expected, they are misaligned
#define TIM1_DMAR_ADDRESS ((uint32_t)0x40012C4C) /* TIM ARR (Auto Reload Register) address */
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
GPIO_InitTypeDef GPIO_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
uint16_t SRC_Buffer[6] = {0x1234, 0x5678, 0xABCD};
int main(void)
{
/* TIM1 and GPIOA clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_GPIOA, ENABLE);
/* DMA clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
/* GPIOA Configuration: Channel 1 as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* TIM1 DeInit */
TIM_DeInit(TIM1);
/* DMA1 Channel5 Config */
DMA_DeInit(DMA1_Channel5);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)TIM1_DMAR_ADDRESS;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)SRC_Buffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST;
DMA_InitStructure.DMA_BufferSize = 3;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel5, &DMA_InitStructure);
TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (SystemCoreClock / 24000000) - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
/* TIM Configuration in PWM Mode */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 0xFFF;
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
/* TIM1 DMAR Base register and DMA Burst Length Config */
TIM_DMAConfig(TIM1, TIM_DMABase_CCR1, TIM_DMABurstLength_3Transfers);
/* TIM1 DMA Update enable */
TIM_DMACmd(TIM1, TIM_DMA_Update, ENABLE);
/* TIM1 enable */
TIM_Cmd(TIM1, ENABLE);
/* TIM1 PWM Outputs Enable */
TIM_CtrlPWMOutputs(TIM1, ENABLE);
/* DMA1 Channel5 enable */
DMA_Cmd(DMA1_Channel5, ENABLE);
/* Wait until DMA1 Channel5 end of Transfer */
while (!DMA_GetFlagStatus(DMA1_FLAG_TC5))
{
}
/* Infinite loop */
while(1)
{
}
}
2024-05-21 9:17 PM
What do you mean by "misaligned"?
Read out and check/post content of TIM and DMA registers.
JW
2024-05-21 10:58 PM
"misaligned" is
first time
CCR1=0x1234
CCR2=0x5678
CCR3=0xABCD
but second
CCR1=0xABCD
CCR2=0x1234
CCR3=0x5678
And then
CCR1=0x5678
CCR2=0xABCD
CCR3=0x1234
2024-05-21 11:00 PM
You can run my code to see the phenomenon
2024-05-22 2:04 AM
I don't use SPL.
What happens, if you use
TIM_DMAConfig(TIM1, TIM_DMABase_CCR1, TIM_DMABurstLength_2Transfers);
?
JW
2024-09-18 3:04 AM
I'm noticing the same issue in my project. It seems to only happen in the debugger mode when I'm live viewing the CCR changes. Maybe your code works as intended when you aren't checking on it.
I attached a screen recording to show what I mean. I'm basically changing rapidly between 50% duty cycle and 100%. This should look like a stable 75% on the scope. It also does before I go into the live view. Then when I go to live view it starts messing up
2024-09-18 5:36 AM
Nice catch!
Yes, debugging is intrusive - but I did not guess that that might be the case in the original post.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.