2019-02-26 12:12 AM
I use STM32 motor control SDK v5.
Is it possible to set SV-PWM duty cycle to achieve regenerative baraking when I stop motor?
PWMC_SetPhaseVoltage() function will be called when motor start or stop?
Thanks
2021-06-14 11:52 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.