2021-02-15 8:07 PM
I am using a custom board with STSPIN32F0A microcontroller. After assigning pins in the Motor control workbench, I am generating the code. Then I dump the code to the MCU by IDE.
After that 12VReg starts.
To test the motor, I go to Motor control Workbench--> Monitor section. Then I initiate UART communication and the device gets connected.
But here the "Under Voltage fault always persists. Please check the image attached below."
Note: I apply 12V input to run the Motor. Motor Used : Bull Running BR2804-1700kv
Please help me solve this problem. I have been stuck over here for more than 20 days.
THank you
Ritul Shah
Solved! Go to Solution.
2021-02-22 12:01 AM
Hello Dario,
I have been able to solve the issue.
I had a problem with UART communication, which created the problem.
2021-02-16 8:52 AM
I got a very similar issue a year ago , i didnt fix it.
2021-02-19 5:28 AM
@Ritul Shah I have some questions to better understand your setup: If I understood well, you a re using a custom board: which is the GPIO line you are using for reading the bus voltage ? Is it the PB1 as in the STSPIN32F0A evaluation board ?
Which are the values of the resistors for the bus voltage divider ?
Did you tried to sense the line used for bus monitoring with a digital multimeter, just to check whether the expected voltage is present ?
I'm just trying to figure out if it is a hardware issue or a firmware issue...
2021-02-22 12:01 AM
Hello Dario,
I have been able to solve the issue.
I had a problem with UART communication, which created the problem.
2021-06-01 8:52 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.