2014-10-22 4:59 PM
Hello
I'm using an STM32F405 based board (OpenPilot ) and i'm looking to capture 5 input PWM signals over only two Timers . For this , i have to use multiple channels of the two timers . I succeeded doing it with only one channel using the example provided with the standard library . But i could'nt adapt it to a multi channel case . Can someone explain to me how to configure the Timers and how to compute the different dutycyles . An example with more than one channel would help a lot . Thanks. #pwm-duty-cycle-computation2014-12-12 2:16 AM
Ciao
The question is not strictly related to motor control firmware so I suggest to ask it in the general discussion forum regarding STM32 like : Microcontroller->STM32 Software Tools and Firmware Ciao GigiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.