2025-06-05 12:59 AM
Hello ,
I have a steval-ctm010v1 , a STLINK V3 MINIE.
I want to use Motor Pilot Tool .
But J3 on steval-ctm010v1 is DP9 interface (232), and STDC14 on STLINK V3.
How can I do the connection between these ports ?
2025-06-05 1:19 AM
RS232 levels (±12V typical) are not directly compatible with TTL UART levels (0-3.3V or 0-5V).
Source: https://www.theengineeringprojects.com/2018/10/introduction-to-rs-232.html
You cannot directly connect the STLINK-V3MINIE to the DB9 port on the STEVAL board without voltage level conversion.
2025-06-05 5:07 AM
So, should I have another hardware tool i.e. TTL<-->RS232 between STLINK VCP and J3 on CTM010V1 board?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.