2014-04-07 9:06 AM
Hi
I'm working with the STM3240G-EVAL Board and trying to drive a BLDC Motor from Maxon EC-max 30 type 339923 (maxon.com) On the motor side I have Hall sensors and an encoder with 500impulses / turn, 2 channels A+B and the Z channel. I used the ST Motor control workbench to set the parameters and IO PINs. Target Lib is SDK v3.4. I'm wondering why I don't need the HALL sensor signals to detect the correct angle of the motor. My problem is now, that I have not a sine current on the motor phases and i can't change the speed of the motor... How can I tune the PID parameters from the speed controller and the PID parameters of the clarke and park transformation? I really need help as soon as possible because I need to getting run with this motor as soon as possible. I hope that anyone can help me. The Plot from the oscilloscope is from the turning motor, the yellow CH1 is the Hall sensor signal from the phase U of the Motor, CH2 = U, CH3 = V, CH4 = W. Best regards, Dominik #stm3240g2014-05-05 2:05 AM
Ciao Dominik
sorry for the delay, I was fully involved in the development of the new lib. version. If it can help I can try to answer now to your request.2021-06-21 9:41 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.