2020-07-09 12:57 PM
I have a P-Nucleo-IHM03 motor control pack, that includes a G431RB MCU, IHM16M1 driver board, and GBM2804H-100T BLDC motor. I am trying to simply create a project in the STM32CubeIDE that makes the motor turn. I went through the process of creating the project in the Motor Control SDK and then opening the project in the CubeIDE. I wrote the following code in the main function of the main.c file:
MC_ProgramSpeedRampMotor1( 1000, 2000 );
MC_StartMotor1();
The project builds without 0 issues and 0 warnings but when I run the program, the motor does not turn.
Any help or advice is appreciated.
2020-09-14 1:25 AM
Dear MSzos.1
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-06 5:47 AM
Dear @MSzos.1
I guess you don't have to solve this problem anymore, therefore I consider this post closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.