cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding STS pin SPIN32F0A

amol_shinde
Associate

Hi team,

I had made project on Motor control workbench in 5.4.8 where i get serial communication to check the parameter.

if i work on 5.Y.4 where serial port is not active, then how to activate the serial port in 5.Y.4?

if i import the 5.4.8 project in 5.Y.4 then the API is not matched. if i maually type the code in IDE then also 5.4.8 & 5.Y.4 parameters may changed.

can i use same drive_parameters.h and pmsm_parameters.h in 5.Y.4 ? observer & PLL?

The API is same for 5.4.8 & 5.Y.4 or different? if different then what to do to check

If i run the motor in 5.4.8 with same parameter with the debugger in IDE, then debugger gets disconnected and i cannot debug the fault.

Please help into this

Regards,

Amol S.

Email ID : amol.shinde@aplosventures.com

1 ACCEPTED SOLUTION

Accepted Solutions
cedric H
ST Employee

Hello @amol_shinde,

The version 5.Y is deprecated and not supported anymore. The communication protocol used by 5.Y is the one used in the MCSDK 6.

The best advice I can give you is to update your project to MCSDK 6.4.0

Regards

Cedric

View solution in original post

2 REPLIES 2
cedric H
ST Employee

Hello @amol_shinde,

The version 5.Y is deprecated and not supported anymore. The communication protocol used by 5.Y is the one used in the MCSDK 6.

The best advice I can give you is to update your project to MCSDK 6.4.0

Regards

Cedric

Hi, thanks for response.

 

Can I use the 5.4.8 workbench for existing project,

If I had complete the project in 5.Y.4 can I port to the 5.4.8

Need to understand all KP & KI will change, PLL values will be the change for 5.4.8?

Or 5.Y.4 workbench need to shift to 6.4.0 ?

Or Need to tune according to workbench?

Workbench to workbench value changes?

What is workbench changes in 5.4.8 and 5.Y.4 ?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.