2024-02-06 2:05 AM
Hi,
I have following Harware configuration:
- X-NUCLEO-IHM16M1 (STSPIN830)
- NUCLEO-L476RG
BLDC Motor with three analog hall sensors
I'd like to be able to configure your Motor workbench to do the job.
Questions:
- Are the boards X-NUCLEO-IHM16M1 + NUCLEO-L476RG compatible ? I suppose yes
- How would you configure position control for analog Hall sensor with your motorworkbench ?
Do you have any api or docs which might help ?
Many thanks
Younes
2024-03-27 3:44 AM
Hello @Youni,
Please, refer to the position control application note.
As mentioned, this feature is only available with a PMSM motor with quadrature encoder (with index signal).
APIs are also described.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.