cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-IHM03

FMarr.2
Associate III

Hi,

Starting from this development board, would like to know if I can add easily encoder (which one) and if there are example project for a servo driver, I mean code to control speed and position of the gimbal motor.

Thanks in advance

2 REPLIES 2
GMA
ST Employee

Dear FMarr.2,

For the encoder sensor, please check with motor or sensor providers.
Once, encoder is added, go on workbench "Motor" tab, enable "Quadrature encoder" and add "Pulses per mechanical revolution" data and select "Has index pin (Ch Z)" if present.
Go on workbench "Speed Sensing" tab and select "Quadrature encoder" and generate project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Lanese22
Associate

Hi FMarr.2,

 

Have you had any success with this? I just got the same board and have been trying to do the same thing with my encoder. I am using an older quadature encoder and have not had much luck getting things to work.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.