2025-10-10 5:51 AM
I want to add a custom motor under "New_Project" in MC Workbench. As soon as i am clonign previous motors, i am not able to edit it and the edit window is getting closed automatically.
Please suggest me what i should do.
2025-10-13 12:22 AM
Hello @Sanchari,
Using new project on Workbench 6.4.1 and clone motor, it is possible to edit motor parameters.
You can also edit the previous motor .json file (located in ~\.st_workbench\hardware\motor) using a text editor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.