2024-03-25 5:06 AM
Hi,
This is my first post on the forum so my apologies if I’m doing something wrong.
OS:
Windows 10 64-bit
Software:
STM32CubeIDE 1.14.1
Motor Control Workbench 6.2.0
ST Motor Pilot v1.2.4
Hardware:
Dev Kit: P-NUCLEO-IHM002
Control Board: NUCLEO-F302R8
MCU: STM32F302R8
Power Board: X-NUCLEO-IHM07M1
Motor: Bull Running BR2804-1700kv
Problem Description:
The motor does not spin when I run the profiler using Motor Pilot v1.2.4. I can see the motor momentary jerks but it doesn’t spin and consequently the profiler fails. I have followed the profiler setup in ST Motor Pilot v1.2.4 > Help > Profiler Documentation. The profiler firmware is generated. I have compiled and uploaded the generated code with STM32CubeIDE 1.14.1. No errors or warnings are generated. When I start the profiler it hangs at 28% - the motor never rotates. See attached screenshots
In contrast I have no problems when using the Motor Pilot instead of the Motor Profiler. With the Motor Pilot the motor spins and I can adjust the speed from the GUI.
Questions:
Thanks:
If anyone from ST sees this message then I want to say a sincere thank you to ST for providing all the excellent tools, software and documentation – for free! A very intelligent business decision and I’m grateful.
Solved! Go to Solution.
2024-04-03 12:45 AM
Hello Gary_Baldy,
I don't know if this is your case, but it feels like you generated a project with MCSDK 6.2.0, then opened the same project with MCSDK 6.2.1 and re-generated that project into the same folder without changing its name. Am I right ?
In any case, please refrain from doing this, as it generally causes a few issues. Please create a new project or save your project in a different folder / with a different name to ensure a correct generation. If the issue persists, please make sure your CubeMx, CubeIDE and Firmware package are up to date. I generated your project using MCSDK 6.2.1, CubeMX v6.11.0, CubeIDE v.1.13.2 and Firmware package v1.11.4 and had no issue.
2024-03-28 7:04 AM
Hello @Gary_Baldy,
Firstly, thank you for your message.
There is a known issue on WorkBench 6.2 profiler (profiler functional for STM32G4 series only), could you please try with 6.2.1 version?
2024-03-31 1:08 AM
Many thanks for your reply!
I installed 6.2.1 and re-generated the code (using the project attached to my first post). When I compiled the new code I got many errors as shown below so cannot test the profiler. Most seem to state 'undefined reference'. I've tried to solve this but haven't succeeded.
Can you help?
13:33:30 **** Build of configuration Debug for project motor_test_2 ****
make -j4 all
arm-none-eabi-gcc -o "motor_test_2.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\user\.st_workbench\projects\motor_test_2\STM32CubeIDE\STM32F302R8TX_FLASH.ld" --specs=nosys.specs -Wl,-Map="motor_test_2.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/mc_api.o: in function `MC_ProfilerCommand':
C:/Users/user/.st_workbench/projects/motor_test_2/Src/mc_api.c:716: undefined reference to `SCC_CMD'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/mc_tasks.o: in function `MCboot':
C:/Users/user/.st_workbench/projects/motor_test_2/Src/mc_tasks.c:890: undefined reference to `SCC_CheckOC_RL'
..... lines removed here due to 20,000 character limit
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/register_interface.o: in function `RI_SetRegisterMotor1':
C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:559: undefined reference to `OTT_SetSpeedRegulatorBandwidth'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:411: undefined reference to `SCC_SetUnderVoltageThreshold'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:585: undefined reference to `SCC_SetResistorOffset'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:238: undefined reference to `SCC_SetPBCharacterization'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:572: undefined reference to `SCC_SetNominalSpeed'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:220: undefined reference to `SCC_SetPolesPairs'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:1398: undefined reference to `SCC_GetLdLqRatio'
C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:1420: undefined reference to `OTT_GetJ'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:66: motor_test_2.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
13:33:32 Build Failed. 55 errors, 0 warnings. (took 1s.624ms)
2024-04-03 12:45 AM
Hello Gary_Baldy,
I don't know if this is your case, but it feels like you generated a project with MCSDK 6.2.0, then opened the same project with MCSDK 6.2.1 and re-generated that project into the same folder without changing its name. Am I right ?
In any case, please refrain from doing this, as it generally causes a few issues. Please create a new project or save your project in a different folder / with a different name to ensure a correct generation. If the issue persists, please make sure your CubeMx, CubeIDE and Firmware package are up to date. I generated your project using MCSDK 6.2.1, CubeMX v6.11.0, CubeIDE v.1.13.2 and Firmware package v1.11.4 and had no issue.
2024-04-03 1:24 PM
Yes, you are correct I opened an existing 6.2.0 project in 6.2.1 and re-built it.
I followed your advice, updated all software components and created a new MC project and now the profiler works.
Many thanks for your assistance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.