2025-06-29 9:33 PM
Hi all,
I am using the STSPIN32G0252Q chip on a custom board (implements 3-shunt current sensing and back-EMF measurement, alongside the required drive features). I have designed the board in the MC Workbench, and have manually profiled the motor I am using, as the motor pilot tool doesn't support the Cortex-M0+ range.
However I am finding it difficult to know where to start with actually implementing the code generated by the workbench/CubeMX; I can see that all of the control functionality is present, but there doesn't seem to be any documentation on how to actually run a motor using just API/HAL calls, instead of using the motor pilot. I have read the SDK documentation, but while this lists all of the functions and control algorithms it doesn't seem to show what a simple implementation loop would look like. Worse still, there seems to be some conflicting information about what each function does (e.g., whether the MC_StartMotor function needs a speed/torque ramp pre-programmed or not).
Does anyone have any tips to point me in the right direction?
Thanks in advance!
Solved! Go to Solution.
2025-06-30 2:07 AM
Hello DMorris42,
Could you please tell me which version of the MCSDK you are using ?
Also, I would like to know where the conflicting information is located in the documentation, as I can't seem to find the one you are referring to :
| bool | MC_StartMotor1 (void) |
| Initiates the start-up procedure for Motor 1. |
Extract from MCSDK documentation.
The start-up ramp is already computed by the WB given your system's characteristics, but you can change it in WB or after generation in drive_parameters.h or directly in the RevUpControlM1 handler in mc_config.c.
2025-06-29 11:12 PM
mc_api.c contains all the functions to run the motor in different modes and stop motor, this file is sufficient to drive the motor.
2025-06-30 2:07 AM
Hello DMorris42,
Could you please tell me which version of the MCSDK you are using ?
Also, I would like to know where the conflicting information is located in the documentation, as I can't seem to find the one you are referring to :
| bool | MC_StartMotor1 (void) |
| Initiates the start-up procedure for Motor 1. |
Extract from MCSDK documentation.
The start-up ramp is already computed by the WB given your system's characteristics, but you can change it in WB or after generation in drive_parameters.h or directly in the RevUpControlM1 handler in mc_config.c.
2025-06-30 4:17 PM
Hi Gael,
I'm using SDK version 6.4.0.
Ah right, it wasn't clear to me that the startup ramp from the WB was pre-programmed for the motor - from reading the documentation it seemed that this needed to be programmed every time, which I found conflicted with the wiki:
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_Motor_Control
as this doesn't discuss control profile generation.
Thanks for the input!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.