2014-01-23 7:00 AM
ST�s motor control software development kit provides all you need for the development of your motor control application based on the STM32 F0, F1, F2, F4 and now F3 (release v3.4) MCUs. It supports up to two PMSMs using any combination of current reading topologies and speed/position sensors, including sensorless operation. Application development and optimization is facilitated by the PC based MC Workbench software. This GUI sets SDK parameters, real-time access to control variables including their display on a virtual oscilloscope. Gigi #stsw-stm32100-pmsm-foc-sdk
2014-06-05 6:46 AM
On the home page of STSW-32100 the user manual reports already to Version 4.0 of the SDK. There are mentioned more projects for MDKARM we want to use.
UM1080:Quick start guide for STM32F PMSM single/dual FOC SDK V4.0
One is: Installation folder\Project\MDK-ARM\STM32F4xx_Workspace.uvmpwWhere and when can I download the
STSW-32100
FOC SDK Version 4.0? A prerelease is o.k. too.2014-06-11 2:03 AM
Now the Release note are also updated to 4.0, but the download is still 3.4
RN0085:
STM32 PMSM single/dual FOC SDK Release 4.0
Please update the download target too2014-06-11 5:10 AM
This mean that the release is imminent...
Ciao Gigi2014-06-12 2:46 AM
2014-06-12 4:56 AM
The plan is to release it by the end of next week with full support of Keil IDE.
Ciao2014-06-12 10:21 AM
About release 4.0.0
• Drive Management – Added HFI sensor less management – Improved Start-up parameters (start-up rump plotting). – Added AC Input selection • Power Stage – Improved Driving Signals Polarity: Added the possibility to force the same values for all U, V, W drivers simultaneously. • Program features: – Adding Compact/Extend mode: showing/hiding advanced feature. • Minor bug fixeswaiting
......2014-06-23 6:06 AM
2014-06-26 7:47 AM
STSW-STM32100
Version 4.0.0 is out!2014-12-04 12:41 PM
PMSM FOC V3.3 firmware ,
but every time my order is rejected, .. kindly help me...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.