2019-11-29 10:40 AM
Hello,
Using the 48-pin variant (STM32F303CB), the "analog input and protection" pin mapper propose inputs that doesn't exist on the chip (C-port) and doesn't propose available pin (A1, A2, A3...)
Any workaround?
Thank you
2020-09-10 5:56 AM
Dear nicolasbouquet9
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-22 1:39 AM
Dear nicolasbouquet9
OK. I consider this post closed.
Do not hesitate to answer if it is not.
Best regards
Laurent Ca...
2021-03-04 4:30 PM
Hello Laurent,
Sorry to resurrect an old thread. I am actually having this same problem as well, with the STM32F303CB and the STM32G431 (I haven't tried with other chips). Any help would be greatly appreciated.
Also, do you know if the SDK will support more chips from the STM32G4 series anytime soon?
Erk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.