2021-07-06 5:00 AM
What's the mean of this sentence?
"Lookup TIM1_CCER value from table based on phase to commutate bridge" What should i do? in page 5.
Or is there any other documents to understand this topic?
Six-step sensorless BLDC motor drive example software for the STM32™
2021-07-06 8:10 PM
Dear @Samet Yazıcı
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools or what version of those tolls you use (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-07-08 1:03 AM
Dear @sametyazici,
Looking at the document, it is a very old one (2013) which is not aligned with our latest 6-steps examples, nor with the current FW architecture and communication feature.
So, we will recommend you to use the MC SDK, using one of the 6-steps examples as a good starting point.
Best Regards,
PBo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.