2023-01-27 10:39 AM
Greetings Tech Gurus,
I have a Nucleo STM32G431 driving an IHM16M1.
Code is Generated by MC Workbench 5.4.8
I am using serial communication for control from my application.
I want to operate in variable speed mode.
I also want to be able to adjust current limit.
Everything works fine until I send a Set current references frame command.
It seems like it switches to torque control mode and accelerates to max rpm.
If I send an Execute ramp frame after that, it switches back to speed mode and
resumes running at speed set in the Execute ramp frame.
Is it supposed to switch to torque mode?
Is there any way to prevent it from doing so?
Thank you,
-Jim
2023-02-01 1:17 AM
Hello,
According to User manual UM2392, on "Motor control API" chapter "Which control mode is active depends on the last programmed reference", then using a current reference API, "torque mode" is selected.
You can handle the current limit via the "Over Current Protection" box on Motor Control WorkBench.
Best regards.
GMA
2023-02-02 9:57 AM
Greetings GMA,
Thank you for your response.
I'm using the serial UI motor control protocol defined in user manual UM1052 to control the motor from my application. My question would be, is there a way to change the current limit in speed control mode thru the serial UI during run time?
Thank you,
-Jim
2023-02-07 6:14 AM
Hello,
From my point of view, there is no easy way to handle it in a dynamic way.
To sum up, MC_SetCurrentReferenceMotor1 sets the used current, and then torque mode is used.
If you want to limit the current on acceleration phase for example, you can use a lower value of "nominal current" on motor definitions side or use a longer acceleration period.
Hope that it helps...
Best regards.
GMA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.