2018-10-16 12:09 AM
I am able to generate a IAR workbench workspace from MC workbench after setting all the parameters but I am stuck.I am generating a 490Hz PWM signal with 50% duty cycle but the motor doesn't rotate.Is it possible to change the PWM frequency in MC workbench? Am I making some other mistake?
2019-04-05 1:15 AM
Hi,
sorry for this huge delay.
Do you have solved the issue mentioned ? Please upgrade the SW with X-CUBE-MCSDK and for PWM management please visit the section " Drone Zone" in this forum.
BR
Giuseppe Scuderi
2021-06-22 2:11 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.