2020-06-18 12:21 AM
Our motor driver need auto update parameter.
Where is st motor profile detail flow figure. or open source code?
Solved! Go to Solution.
2020-10-26 5:50 PM
I fixed it. I measure pluse current (3 points). than calcuate R and L. It is sloved.
2020-06-30 12:46 AM
Dear YLin.1,
The source code is not available,
I will check about the flow figure,
Claire
2020-10-14 7:50 AM
Dear @YLin.1
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-26 2:51 AM
Dear @YLin.1
I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting an answer.
Best regards
Laurent Ca...
2020-10-26 5:50 PM
I fixed it. I measure pluse current (3 points). than calcuate R and L. It is sloved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.