cancel
Showing results for 
Search instead for 
Did you mean: 

how to connect X-NUCLEO-IHM08M1 with NUCLEO-F446RE

Shubham08
Associate III

Initially i powered the board by following the steps provided by the st motor profiler. I have tried with Motor control work bench 5.4.8 and 6.3.0. First i tried with 5.4.8 the motor profiler was running but stopped at 94% indicating to check the MAX RPM part in the motor control profiler. After that i tried with 6.3.0 but in that the code was generated with error, so while compiling it was showing some.h file not found. Again when i tried with 5.4.8 it is showing over current error at starting only.

Shubham08_0-1724401483586.png

Shubham08_1-1724401502424.pngShubham08_2-1724401528145.png

Shubham08_3-1724401550618.png

Additionally i have removed C5,C3 and C7  as suggested in the vedio

 https://youtu.be/qB7jJqCr72U?si=K-o0B9kFZTxo9RVP  

 

2 REPLIES 2
GMA
ST Employee

Hello @Shubham08,

Concerning the code generation with 6.3.0, if your error is "Attr not supported : Dmpu", please do not take it into account as mentioned in this post and please proceed with generated code (if generation ends with main.c generation).
For the OverCurrent error, what Profiler Max Current APK value have you set? 
You can try decreasing it...

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

but motor profiler is not working that is the first issue even if i reduced the current value

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.