2018-05-14 7:13 AM
Hi,
When not using the motor profiler and instead writing all details by hand into the Motor Control Workbench (with Hall Sensors, Manual editing of PI variables disabled) at Motor - Parameters, there are fields for Inertia and Friction. So far, so good. Just the units are a bit confusing:
Inertia: uN*m*s2
Friction: uN*m*s
I thought that inertia had the units kg*m² and friction N*m, which I wasn't able to match with the given units.
Any clues how to do this right? Also does u stand for micro in this case or for something else?
Thanks,
Martin
Solved! Go to Solution.
2018-05-15 7:30 AM
Hello Mr. Martin,
Yes sure, you are right, in that form the units are a bit confusing. Thank you for reporting this problem, we will try to improve them.
About 'u', yes, it
stands for micro (1E-6)
and
`N` stands for Newton the
SIunit of Force(
1 Newton is equal to 1 kg
·
m·
s-2)https://wikimedia.org/api/rest_v1/media/math/render/svg/07948745d4db778de832933915f84be8bd9b4ded
So: N·m·s² = kg·m²
Hope this can help.
Best Regards.
2018-05-15 7:30 AM
Hello Mr. Martin,
Yes sure, you are right, in that form the units are a bit confusing. Thank you for reporting this problem, we will try to improve them.
About 'u', yes, it
stands for micro (1E-6)
and
`N` stands for Newton the
SIunit of Force(
1 Newton is equal to 1 kg
·
m·
s-2)https://wikimedia.org/api/rest_v1/media/math/render/svg/07948745d4db778de832933915f84be8bd9b4ded
So: N·m·s² = kg·m²
Hope this can help.
Best Regards.
2018-05-15 11:27 PM
Nice, Palano. That works perfectly for the Inertia.
Can you also explain how to make sense of N*m*s instead of N*m? Or explain what kind of friction is meant here if not frictional torque?
Many thanks!
2018-05-17 7:43 AM
Hello Mr. Martin,
As you correctly said, the unit of measurement of the Friction Torque is [N·m]
The item required in the form of our tool, measured in [N·m·s], is the coefficient of the Friction Torque.
Friction
Torque
[N·m] :
TF= β·�?‰where �?‰
is the angular velocity (Rad/s) and β
is the coefficient required by MC-Workbench [N·m·s].
If not directly available, the the ST-MotorProfiler could be an effective way to detect it; in alternative, use external equipment like torque meter and speed meter.
With Best Regards.
2021-06-27 6:26 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.