2022-12-15 1:56 AM
Below is a copy of a warning found within the PID-controller of MC-SDK 5.Y.4.
We have a Cortext-M4 based board so I guess the warning text is a copy-paste and I should not care that it mentions Cortex-M3..
/* WARNING: the below instruction is not MISRA compliant, user should verify
that Cortex-M3 assembly instruction ASR (arithmetic shift right)
is used by the compiler to perform the shifts (instead of LSR
logical shift right)*/
//cstat !MISRAC2012-Rule-1.3_n !ATH-shift-neg !MISRAC2012-Rule-10.1_R6How can we check if the compiler uses ASR and not LSR in these situations?
Solved! Go to Solution.
2022-12-15 2:00 AM
Generate a listing file and inspect it?
2022-12-15 2:00 AM
Generate a listing file and inspect it?
2022-12-15 3:18 AM
Thanks for the reply.
Never inspected a listing file, but did my best.
First, found the STM32 Cortext-M4 Programming Manual (PM0214) and looked up Arithmetic Shift Right in the Instruction Set table (Table 21). Further read the reference chapter for that instruction.
In the listing file, I found a section for PI_Controller function and copied it for simplicity's sake to a new editor. Searching for both ASR and LSR. Comparing the lines for ASR with the PM0214 tells me that ASR is used some places, although my experience with assembly code is zero so I cannot relate the specific line in listing file with actual C code. My search for LSR ended up with zero hits.
Is it correctly of me to assume that the function uses ASR for the specific shift operation?
2022-12-15 3:37 AM
This MISRA caution is about making a definitive determination, the danger is in making assumptions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.