cancel
Showing results for 
Search instead for 
Did you mean: 

Function of U5 (ST890DTR) in B-G431B-ESC1 Development Board

Ankitesh
Associate II

1. In the B-G431B-ESC1 development board, there is a component labeled U5 (ST890DTR) in the circuit. Could you please explain the exact purpose or function of this component in the board’s design?

2. If the U5 (ST890DTR) component is removed from the B-G431B-ESC1 development board, what types of issues or malfunctions could occur? Would the impact be considered minor, major, or critical to the board’s operation?

4 REPLIES 4
GMA
ST Employee

Hello @Ankitesh,

Refer to ST890 page for feature description and documentation.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Ankitesh
Associate II

Dear Sir,
I have already the B-G431B-ESC1 development board, I just want to know about U5 (ST890DTR) in the circuit. So that i can remove it. 

 Can you please answer the questions i had mentioned? That will help me.

Any reason why you want to remove U5 IC?

Hello @Ankitesh,

Take the time to read the documentation of the ST890DTR, and since it is a protection for the board, it is not recommended to remove it.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.