2016-11-21 10:11 AM
Hello.
I want to use this SDK with encoder.I configured the encoder as the main sensor and programmed the EVB (I am using the P-NUCLEO-IHM001).The motor starts rotating, but then I turn the encoder wires off it continues to rotate at the right speed. Why?In this situation I'm pretty sure it would give a fault...I have the feeling that my encoder is not being used and the motor starts with sensorless and never enable encoder reading.Thank you. #encoder #sdk-4.32016-11-22 1:43 AM
Could it be something related to this?
2016-11-22 2:10 AM
2016-11-30 2:32 AM
Solved!
2016-12-08 12:46 AM
How solved?
2021-06-15 4:34 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.