2025-07-24 3:36 AM
Hi ST Team,
I'm using the EVSPIN32F0601S3 development board and attempting to control a BLDC motor via Motor Control Workbench 6.3.0 and Motor Pilot 6.3.0.
Everything connects successfully when I open Motor Pilot — the board is detected, and parameters are correctly loaded. However, as soon as I press the "Start" button to run the motor, Motor Pilot immediately disconnects from the board. There's no error message aside from the disconnect itself.
What I've tried so far:
Verified UART connection (using STLink onboard)
Ensured the power supply to the board and motor is stable
Reflashed the firmware generated by Workbench
Tried different USB cables and ports
Rechecked motor parameters (voltage, current, sensor type, etc.)
Environment:
Motor Control Workbench & Motor Pilot 6.3.0
EVSPIN32F0601S3 with STSPIN32F0601
BLDC motor (sensorless)
Windows 10
It seems like the firmware crashes or resets when the motor is commanded to start, leading to a loss of communication with Motor Pilot.
Has anyone else experienced this or have suggestions on how to debug further?
Thanks in advance!
2025-07-24 6:01 AM
Hello @Sunil_Kumar_G,
It could occur when the MCU is overloaded. Try using a lower PWM frequency value.
With a debugger, you can check the MCI[] table which contains the following:
2025-07-30 2:17 AM
Hello St Team,
No errors have occurred. Only my UART is getting disconnected, while the motor is running fine.
2025-07-30 2:24 AM
Hello @Sunil_Kumar_G,
It could occur if the MCU is heavily loaded. Could you try reducing the PWM frequency?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.