2024-07-11 4:04 PM
Hi,
I am confused on how I can get this board: EVLDRIVE101-HPD, to work.
For context, I am simply trying to get the EVLDRIVE101-HPD to run a compressor motor.
From my understanding, I believe I need to generate the code/firmware through MCSDK workbench and then compile the code through an IDE (im using STM32CubeIDE) into the EVLDRIVE101-HPD board with the STM32G071KBT. However, both softwares do not have the board (EVLDRIVE101-HPD) as an option in the setup.
I have the board's JSON file which I believe can be imported in the MCSDK workbench but need further instructions on how?
Could I please have some general help with this? As well as clear instructions on how to get this board to work with my motor?
Any help will be appreciated. thanks!
Solved! Go to Solution.
2024-07-12 9:14 AM
Hello @mitch1,
With MCSDK6.3.0, please refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation", click on "Motor Control Workbench User Manual".
The EVLDRIVE101-HPD is selectable since at "New Project>General Info" Inverter is selected.
2024-07-12 9:14 AM
Hello @mitch1,
With MCSDK6.3.0, please refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation", click on "Motor Control Workbench User Manual".
The EVLDRIVE101-HPD is selectable since at "New Project>General Info" Inverter is selected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.