2025-06-19 11:10 AM - edited 2025-07-07 11:57 PM
Hello, @Peter BENSCH @Cristiana SCARAMEL @TDK @Amel NASRI
I recently came across the easySPIN library for controlling a stepper motor using the L6474 driver. The library provides two board options: STEVAL_PCC009V2 and STM32_VL_Discovery.
I am using the STEVAL_PCC009V2 code and have selected the STM32F103C8 as the target in uKeil. The code compiles successfully and flashes without any errors.
I have connected SPI2 and other required pins (SCK, DIR, STBY_RESET, and FLAG) as defined in the easyspin.h file. However, the motor does not move.
The main.c file contains motor functions such as eMotionControl_GoTo(-65);. I am attaching the relevant files for your reference. Kindly review and let me know if I am missing something.
Thank you!
2025-07-18 1:29 AM
Hello @SannanAli ,
I suggest to use the X-CUBE-SPN1 software package
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.