2024-10-23 10:30 PM
hi,
I used an example in mc workbench because I could not select my controller board as it is not separately available. then I generated a project for excuse and cube ide, I ran the program and had to create a hex file by adjusting settings and flashing that hex file on the controller. still, the motor profiler is unable to read the controller and I am receiving a firmware error. can you provide a proper firmware file for my project, I have tried everything.
Project name9example (example used): Electronic Speed control on B-G431B-ESC1 kit
MCU: STM32G431CB
type: algorithm- FOC, topology- three shunt resistors
Control: B-G431B-ESC1
Powers: B-G431B_ESC1
Motor: SM-PMSM
Description: Electronic speed control on B-G431B-ESC1 kit and SM-PMSM SHINANO motor. (I am using custom made SM_PMSM motor)
then I tried using older versions of mcsdk, the motor profiler reads the boards and then stops, giving the same error
error: firmware error: the firmware detected is not a profiler firmware, please generate a profiler framewire project with the MC workbench
I used this to generate code in IDE, which I flashed on the MCU. However, the motor profiler is still having a firmware error. How can I resolve this?
Solved! Go to Solution.
2024-10-24 12:14 AM
Hello @madhavP,
Did you generate the project with the motor profiler feature enabled as described in documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab, "Motor Profiler Application Note" on "Figure 3 : MCSDK WB Motor Profiler project flag"?
2024-10-24 12:14 AM
Hello @madhavP,
Did you generate the project with the motor profiler feature enabled as described in documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab, "Motor Profiler Application Note" on "Figure 3 : MCSDK WB Motor Profiler project flag"?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.