STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Motor Pilot bugging. Is my Workbench configuration wrong?

Hi, I'm getting some nonsense values in Motor Pilot under "MC Configuration". It says there is no max app current or voltage, and my PWM frequency is something ridiculous. I've tried changing it to 25kHz and 20kHz, and these were the readings. I've n...

0693W00000Y9kcPQAR.png 0693W00000Y9kcUQAR.png 0693W00000Y9kdDQAR.png
Popeye by Associate III
  • 3736 Views
  • 7 replies
  • 0 kudos

How to use Motor Profiler 6.1.0

Since ST Motor Control SDK 6.1.0, the Motor Profiler app has been integrated into MotorControl Workbench. Unfortunately I was unable to find how the new version of Motor Profiler can be configured and used. Wondered if anyone has used Motor Profiler ...

DAlek by Associate II
  • 1979 Views
  • 3 replies
  • 0 kudos

How to change between FOC and 6-step algorithm?

This might be the most banal question you've heard all day. I don't know if it's even possible, but I thought there is the option of switching between the two. I'm using hall sensors for my application, so it probably doesn't matter much either way.W...

Popeye by Associate III
  • 2262 Views
  • 4 replies
  • 0 kudos

Why do I need to specify current?

Hi. I'm getting fault after fault trying to get my motor to run. FAQ document says to change ramp-up parameters. Why? Why should I specify any current values? I want the motor to get to a certain speed, and the control algorithm should handle the MOS...

0693W00000Y9iW0QAJ.png
Popeye by Associate III
  • 793 Views
  • 0 replies
  • 0 kudos

Can I control a BLDC motor based on encoder counts?

Hello.I'm using Nucleo F446re and IHM07M to control a BLDC motor. It has a built-in 2000 pulse quadrature encoder. The MCSDK version is 5.4.8. I tried the position control method and it works fine. However, it only allows me to control the motor base...

MUddi.1 by Associate
  • 1281 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.