2026-01-08 11:54 AM - edited 2026-01-08 1:55 PM
Hallo,
i try to run an B-G473E-ZEST1S with STEVAL-LVLP01A. I generate code with the default setting from MCSDK 6.4.1., STM32CubeMX 6.16.1, STM32 FW V1.6.1 (Recommended)
I changed nothing on the board hardware or MCSDK settings, i choose the 2 boards and generate code, but after startup I end always in an "<signal handler called at 0xffffffe9>".
The error occours after MX_NVIC_Init(); without MX_NVIC_Init(); the code is running, so it has something to do with the interrupts, but I don't get it.
Does anyone know what could be the cause of this error? Has anyone successfully used this board with the MCSDK 6.4.1?
Thank you!
Solved! Go to Solution.
2026-01-08 1:57 PM
I have found it, it was the missing boot 0 jumper on the board.
2026-01-08 1:57 PM
I have found it, it was the missing boot 0 jumper on the board.
2026-01-12 4:48 AM
Hello @Raphael_Ko,
Thank you for your feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.