2025-09-17 3:52 AM - last edited on 2025-09-17 4:00 AM by Andrew Neil
Hi,
I am using W25Q64JV NOR flash of size 8MB on ST STM32U5A9ZJ board. On the flash I have created a file system using LevelX and FileX. I have enabled fault tolerant option in FileX. I am writing 128bytes of data every 500ms to a file. Initially the write operation is taking around 70-80 ms, however after some time (after around 3000 writes) the write operation occasionally is taking around 3-4 seconds. This is after every few writes. Following is the fx_media_format parameters I have used
status = fx_media_format( &flashMedia,
fx_stm32_levelx_nor_driver,
reinterpret_cast<VOID *>(LX_NOR_OSPI_DRIVER_ID),
reinterpret_cast<UCHAR *>(mediaMemory), sizeof(mediaMemory),
"FLASH_DISK",
1, // Number of FATs
32, // Directory Entries
0, // Hidden sectors
(0x800000 - 0x10000)/ 0x10000, // Total sectors minus one
512, // Sector size
8, // Sectors per cluster
1, // Heads 1
);
Could anyone please let me know what I might to improve the performance? My goal is to complete the write operation of 128 bytes under 100ms in any circumstances. Thanks in advance.
Goutam
Edited to apply source code formatting - please see How to insert source code for future reference.
2025-09-17 4:02 AM
> (after around 3000 writes)
Do you or LevelX / FileX take care of wear leveling?
If you're doing your tests a few times you easily reach > 100k writes, and most flash memories getting problems from then on.
So check the flash's datasheet!
2025-09-17 4:13 AM
Probably the code erases flash sectors as needed, once a write access crosses over into the next sector.
This sector erase can take dozens or hundreds of milliseconds, and is temperature and wear-dependant.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.