2016-05-16 12:29 PM
I am new to STM32 MCU's so I got the STM32F0 Discovery board to familiarize myself. I am attempting to use STM32 Cube code generator.
The STM32 Cube creates an IRQ handler for each interrupt I activate that look like this:/*** @brief This function handles TIM3 global interrupt.*/void TIM3_IRQHandler(void){ /* USER CODE BEGIN TIM3_IRQn 0 */ /* USER CODE END TIM3_IRQn 0 */ HAL_TIM_IRQHandler(&htim3); /* USER CODE BEGIN TIM3_IRQn 1 */ /* USER CODE END TIM3_IRQn 1 */}My question how do i decide whether to put code in the top or bottom part of the user code sections. Thanks in advance for the help! #interrupt #irq #smt32cube #m02016-05-24 7:21 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-08-22 10:54 PM
http://tinypic.com/view.php?pic=28whrx4&s=9#.V7voU_krKUk
I also am confused, can anybdy input some knowledge and kindly answer this image question jpeg I have attached. Thanks. ________________ Attachments : GENERAL_QUESTION.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtrV&d=%2Fa%2F0X0000000aY2%2Ff39p2U6IFoKYQ2_BL8gYSpvtv1jYYgaPvTUsl5XNiCk&asPdf=false2016-08-23 4:50 PM
HAL adds a lot of abstraction. The processor calls the basic IRQ_Handlers described in the Vector Table, these in turn call an object handling form within HAL, ie it passes an internal structure down. IRQ_Handlers can't return values, the process destroys the context as it returns to normal execution.
C functions can return all manner of things, these can typically be up to 64-bit here, and can include structure pointers, enumerated values and typedef'd variables. Returning enumerated values rather than #defined ones allows the debugger can actually decode the types properly. If you can cut-n-paste text don't use graphics.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.