2023-08-24 7:05 AM
Hi,
I'm working on a tool that must be armed only in a proximity range of 0-5mm with different target materials.
The sensor has a protection glass(1mm thickness) 3mm away so the real distance 0mm of the reported measures starts at 4mm from sensor.
I had chosen the VL53L4CD for its precision in range 1-200mm but, with metal target (grey and reflecting), but I measure those values:
Real distance from glass[mm] Measured distance[mm]
0 18
5 6
10 1
15 4
20 18
25 25
There is a non-linearity in the distances that i want to consider to arm my instrument and also without the glass the behaviour persist..
With other target materials as paper, black target, white target, teflon etc. there aren't non-linearity.
I'm using standard API with VL53L4CD_PROFILE_CONTINUOUS and TIME_BUDGET = 15ms.
Could you give me some suggestions?
Thanks for your time,
Andrea
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.