2011-07-09 2:13 PM
Hello!
I've adjusted the Virtual Com Port example from the FS USB Library V3.2.1/V3.3.0 to my needs on STM32F103RC. It works. As a preparation to merge USB CDC and Mass Storage (suggestions and solutions are welcome!) I'm trying now first to ''move'' the COM communication to the endpoints 4,5 and 6 instead of the origin 1,2 and 3 in the example. It does not work. Exactly, the Virtual COM does appear under Win7 (endpoint 0 is untouched) but no communication occures. I think I've missed some substitution or misunderstood the allocation of the endpoints. Could anyone share with me a kind of check list, what changes/substitutions should be made to the application part of the USB library (usb_conf.h, usb_desc (.h, .c),usb_prop (.h, .c), usb_endp.c, usb_istr (.h,.c) and
usb_pwr (.h, .c)) to get the communication over EP4, EP5 and EP6? TIA. #usb-endpoints-change #virtual-com-port-alternative-endpoints #composite-virtual-com #usb-cdc-rl-usb-severe-mistake
2011-07-23 1:41 AM
FYI: while playing with the RL-USB from KEIL on the board with STM32F103RC
(similar to MCBSTM32) I might have found a severe mistake in the KEIL ''USB-Driver''. The driver file is ''usbd_STM32F103.c'' and is normally to copy and custom in the project.Symptoms: firmware with USB CDC implemented stalled as soon as the USB cable was unplugged on the self powered device.Found: the USB interrupt stayed pending because of ESOF flag set while in the ISR there was no branch processing this flag. USBD_Reset() enables the interrupt on this flag along with SOF. The part of the code doing this looks like:CNTR = ....
((USBD_P_SOF_Event != 0) ? CNTR_SOFM : 0) |
((USBD_P_SOF_Event != 0) ? CNTR_ESOFM : 0); The interrupt occurs as soon as and only when the USB is unplugged.Suspicion: ''copy and paste'' mistake. Besides, I suppose, KEIL programmers might have tested the code on the device that was bus powered only (supply gone, problem gone).Solution: the last line setting CNTR_ESOFM has been removed; firmware works. My question to USB gurus: how the handler for ESOF should look like if I decide to process it?
2011-07-25 12:18 PM
sorry for the test -- I was unable to post a new message
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.