2019-06-25 1:04 AM
Hi
I plan to include the USB input of STM32F303 and am not willing to power up the board with the +5V of Vbus. The board will be supplied permanently with 3.3V. Is it necessary the connection of Vbus? If yes how i should connect it to the +3.3V Vdd of STM32?
Thanks
2019-06-25 1:20 AM
You need VBUS to detect USB-plutg/unplug.
2019-06-25 2:36 AM
Thanks.
So i should use one of the many circuits i found in Google, e.g. this with the FET that is connected among +3.3V Vdd ---> Res 1.5K----> D+ input with its gate driven by the Vbus +5V ? Is that OK?
2019-06-25 2:48 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.