2019-05-08 11:38 AM
Hi
Making a very simple freeRTOS project with only one timer on a bluepill
the LED is blinking with 1000 hz = tick rate and not with 1 hz as programmed ...
What did i do wrong ?
/* Create the timer(s) */
/* definition and creation of myTimer01 */
osTimerDef(myTimer01, Callback01);
myTimer01Handle = osTimerCreate(osTimer(myTimer01), osTimerPeriodic, NULL);
/* USER CODE BEGIN RTOS_TIMERS */
xTimerStart(myTimer01Handle,1000);
/* USER CODE END RTOS_TIMERS */
/* Callback01 function */
void Callback01(void const * argument)
{
/* USER CODE BEGIN Callback01 */
HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
osDelay(50); //// this just to reduce the blink freqvenzy so i can see it do blink
/* USER CODE END Callback01 */
}
2019-05-08 11:56 AM
solution was to do xstarttimer in default task
void StartDefaultTask(void const * argument)
{
/* USER CODE BEGIN 5 */
osTimerStart(myTimer01Handle,1000);
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END 5 */
}
but then CUBEMX are not correct because it says
/* Create the timer(s) */
/* definition and creation of myTimer01 */
osTimerDef(myTimer01, Callback01);
myTimer01Handle = osTimerCreate(osTimer(myTimer01), osTimerPeriodic, NULL);
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
START TIMERS ...that is wrong !!!!
Hjalmar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.