2023-05-04 1:09 AM
I tried flashing firmware using System Bootloader earlier and got it working only one time, you can refer to my previous post. By exploring found that there is a similar kind of bootloader that work in the Main Memory.
I am getting some hands-on with the same. But it is giving me the same error as in the case of the System Bootloader. I am making use of USART (PA9 and PA10) to flash the firmware. Open Bootloader is located by default in the 0x08000000 to 0x080003F0.
I have a few questions
/* Infinite loop */
while (true)
{
OpenBootloader_ProtocolDetection();
}So, how the new firmware written will be executed if it does not come out of this infinite loop?
3. System Bootloader resides in System Memory which is 28KB wide and said to be ROM-based memory. Do the entire 28KB is utilized by System Bootloader?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.