2016-07-11 7:44 PM
I's using STm32CubeMX to generate code for 429's OTG-FS. But I find there is a grayed option 'USE_BUFF_WO_ALIGNMENT', it's fixed to 'Enable', and on USB_OTG_FS configuration wizard, the 'Enable internal IP DMA' is fixed to 'Disable', why? Does it mean F429 OTG-FS can't use DMA?
#dma #otg2016-07-13 6:31 AM
Hi,
DMA transfer is only available in HS mode, but you can using the OTG HS in Full Speed mode to achieve your goal.You can look into the STM32F4 and , that can be helpful for you.RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.