2010-06-16 12:23 AM
USB_virtual com port
#virtual-com-port #seteptxvalid #usb2011-05-17 4:54 AM
Hi,
I would like to read more about it what you explain but I couldn't find. Might you give me some advice. r,r2011-05-17 4:54 AM
> I would like to know how to check if USB on PC is avaliable to recive new data
Is it Windows ? Just after enumeration, Windows CDC driver (usbser.sys) starts to poll the device bulk IN endpoint (EP). This polling occurs regardless PC application opens the COM port or not. The data sent from the bulk IN EP is stored to the RX buffer on usbser.sys, until RX buffer overflows. The data is still there when a PC app opens the COM port. If your device want to know the timing when a PC app opens / closes the COM port, the PC app explicitly sends a sign to the device. For example, a) Toggle DTR signaling, or b) Send a specific character over the bulk OUT endpoint.> or USB tx buffer on STM32 is empty. a) when GetEPTxStatus() returns DEV_EP_TX_NAK, the endpoint is empty OR b) When a transaction completes on EP1, EP1_IN_Callback() is called from USB ISR (USB_Istr()) In this callback, you may raise a flag to show the endpoint is empty. or, when the transfer size is greater than full-packet size, second (and later) packet is fed to the endpoint, in this callback. Tsuneo2011-05-17 4:54 AM
Unfortunately, the User manual of STM32_USB-FS-Device_Lib (UM0424) doesn't explain endpoints operation so much, other than the default.
The read/write operation of USB endpoint is almost similar to UART RX/TX. USB endpoint exchanges packet, but UART does a byte. Except for this difference of data size, the coding pattern is the same.
To send single byte to UART TX,
- Check TX flag to know the TX register is empty
- Write to TX register
To send single packet to IN endpoint,
- Check STAT_TX flag to know IN buffer is empty
- Write to IN buffer, and validate it (to show the end of multi-byte write)
To send multi-bytes to UART TX,
- Fill a buffer with data
- Send the first byte to TX, using above procedure.
- On TX interrupt, next byte is passed to TX register from the buffer, until the last byte comes.
To send multi-packets to IN endpoint,
- Fill a buffer with data
- Send the first packet to IN endpoint, using above procedure.
- On IN endpoint interrupt, next packet is passed to IN endpoint from the buffer, until the last packet comes.
When you are aware of this analogy, USB endpoints become familiar with you at all.
For transfer of greater size, you may find this post helpful
http://www.cygnal.org/ubb/Forum9/HTML/001627.htm
Tsuneo
2011-05-17 4:54 AM
Hi,
I write simple test for virtual com port. while (1){
if(GetEPTxStatus(ENDP1) == EP_TX_NAK && BUTTON_PRESSED)
{
USB_SIL_Write(EP1_IN,''test'',4);
SetEPTxValid(ENDP1);
}
} I plug my device into PC. Open port(virtual com port). When I press BUTTON the message is sent over usb and device EP status appear EP_TX_NAK so I am able to transmit data again . But if I press button after a while (20sec or 1minute later). My device stay in EP_TX_VALID mode. And I am not able to transmit data again. To see it on my PC. I try to change code to:while (1)
{
if(BUTTON_PRESSED)
{
USB_SIL_Write(EP1_IN,''test'',4);
SetEPTxValid(ENDP1);
}
} Now I don't understand. I received data if I press button. But only if I press Button once per second. If I press it later the IF statement is executed but I can't receive or see data on my PC. r,S
2011-05-17 4:54 AM
2011-05-17 4:54 AM
Hi,
I have the following. How often usb can send data(periodically(64 databuffer per ms)? while (1) { if (BUTTON_pushed) { while(BUTTON_pushed){}; BUTTON_PRESSED = 1000; }if(GetEPTxStatus(ENDP1) == EP_TX_NAK && BUTTON_PRESSED){
USB_SIL_Write(EP1_IN,''test'',4);
SetEPTxValid(ENDP1);
}
BUTTON_PRESSED--;
}
} r,S
2011-05-17 4:54 AM
What device are you using: STM32F105/7xxx or STM32F101/3xxx ?
If you use STM32F105/7xxx devices, no need to check on EP status, the write operation is managed by a FIFO, and you can write as many data as you want till the FIFO is full (and even when it is full it rolls back to first address I guess).How often usb can send data(periodically(64 databuffer per ms)? Yes, theorically it should be able to send, in full speed, 64 bytes/frame/endpoint (64B/ms).2011-05-17 4:54 AM
> I have the following. How often usb can send data(periodically(64 databuffer per ms)?
Transfer speed of bulk is proportional to the transfer size.
- When you send 4 bytes transfer, like above code, you'll get 4 bytes/ USB frame (1ms)
- When you send 300 bytes transfer, split into 5 packets (64 x 4 + 44 bytes), you'll get 300 bytes / frame.
Theoretical max is 19 full-size packets (64 bytes) / frame for full-speed bus.
Of course, bulk transfer is ''best effort'' type, full bandwidth is not always available.
If any other device on the bus has interrupt or isoc endpoint, the endpoint gets priority than the bulk endpoint. All of active bulk endpoints on the bus share the rest.
Tsuneo
2011-05-17 4:54 AM
Hi,
I use stm32f103rc r,SWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.