2025-01-23 6:43 AM
i'm trying to learn about ST USB LIBRARY AND CLASSES . i tried to run an example on my stm32h7a3ZI-Q board but i didn't succeed . i tried the HID class to make the board act like a mouse . i really copied the MOOC tutorial video step by step and the code was compiled with 0 error but when i run it ,nothing happen when i press the blue button( i checked it in an other led blinking project and the button is working fine) . so i tried the keyboard tutorial from the mooc tutorial also but the serial monitor didnt show anything . i checked the internet and it appears the board lacks a VCP so i tried to run a project with the CDC class to simulate a VCP to link the board with the serial monitor but also it didn't show anything despite code was clean from any error and im pretty sure i used the right functions(CDC_TRANSMIT_HS) . i used CN1 if this helps . so is there any guide? . i really didnt now where i went wrong . i didn't find any article that guides me to run a project step by step like (webcam on h747i for example) i also tried the USB _standalone project .in the readme they said i only need to plug the board and run the project but when i did nothing happend . the cursor didnt move when i clicked the blue button.
here is the video i followed : https://youtu.be/6MJJwDKsKsc?si=t5FA9LdYFcq1V_7C
Please Help
2025-01-23 8:44 AM
Hi @yessine
Are you using NUCLEO-H7A3ZI-Q? Did you check the example provided in cube firmware?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-23 11:21 AM
yes im using that board . and i tried the example provided. the cursor didnt move despite the code compiled with 0 errors and i managed to run it . the only thing that i didnt follow is that i used the CN1 connector(micro typeB to power the board and run the project ) not the CN13 as mentioned in the readme file because i didnt find the cable that fit CN13 . i mean a normal micro type B cable can fit in the CN13 PORT but he doesnt power the board(so i didnt know if its the right cable or not) . can you provide a picture for the cable that CN13 needs if this may be the problem or is there any jumper that i need to change . i really ran out of ideas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.