2011-06-05 3:58 AM
Hi:
I got stuck trying to use STM32 Connective line controller towork as a USB HOST. If I attach flash drive the device attaching is detectedbut the enumeration is not working. USB Control packet is send but the devicealways returns URB_STALL (as per USB OTG flag). I tried different devices sameresult.
Anyone has any suggestions?
Thanks,
Konstantin
#off-topic #old-thread #usb-host-library-enumeration2011-06-19 11:21 PM
It is gcc 4.5.2.
2011-06-23 3:53 AM
I'm encountering the same issue. Can you share your actual fix ?
thanks in advance
fred
2011-06-23 4:57 AM
Just eliminate the uint16_t_uint8_t type and substitute with uint16_t and change the code where it is being used. Example:
typedef union _USB_Setup
{
uint8_t d8[8];
struct _SetupPkt_Struc
{
uint8_t bmRequestType;
uint8_t bRequest;
uint16_t wValue;
uint16_t wIndex;
uint16_t wLength;
} b;
}
USB_Setup_TypeDef;
I have to warn you that I am still encountering problems with this firmware and it seems nobody ever bothered to test how the code behaves when GCC is used as compiler.
Thanks,
Konstantin
2011-06-24 6:48 AM
This is strange ! Does it mean that GCC is not able to compile/recognise the union...? Changing the union type to uint16_16 will probably affect other parts to code.
By the way, Petrov, can you share with us the firmware you want to run ? Mass-storage or HID ? Do you have any other compiler, for which the workspace is already available in library ? I tried mass-storage and HID both with IAR, it works fine ! The project was already available in the lib ;-))2011-10-27 10:37 PM
Hi alokm
Did you connect USB keyboard? I tried to connect to keyboard with STM3210C-Eval board but didn't get keyboard data. Get VID, PID and Enumeration was done propely. What's wrong? Thanks.2014-07-26 5:58 AM
2014-07-26 8:48 AM
Please don't dig up 3 year old posts when you have already posted in the here-and-now with your own thread.
Your thread will either be answered by current participants in the forum, or it won't.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.