2022-11-15 10:46 PM
Hi,
I am trying to activate the USB Audio as a microphone profile.
This feature already implemented for STM32L4 family, and it works correctly.
I am trying to run the same USB stack on EVB B-U585I-IOT02A board, I see that the device is detected as USB microphone, but the dataIn() callback is not called. When I am checking HAL_PCD_IRQHandler it is not called any more after the initialization process.
I understand there are some differences in the USB module between the L4 to U5 family, but still I don’t the get reason why dataIn() is not called.
I will appreciate your assistance on that issue.
Avi
2023-01-16 8:55 AM
Hello @Community member and welcome to the community,
make sure that the USB Handler interrupt is enabled.
Mohamed Aymen
2023-01-17 12:41 AM
Hello
Can you please specify the STM32L4 example?
Mohamed Aymen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.