2013-09-01 5:05 AM
Dear All,
I'm working on use RAM memory from STM32F205 on mz custom PCB to run code from STM32_USB-Host-Device_Lib_V2.1.0 under Iar workbench. From mass storage device example workspace I removed all board specific calls lik LCD logger and SD card and changed them to write/read from my uin8_t usbDisk[0x1000] buffer placed in RAM. I can see that device is connected in device manager Win7 without any yellow marks, but when the OS wants to format removable device I got ''Windows was unable to complete the format''. I can see that some SCSI commands are invoked like: SCSI_INQUIRY, SCSI_READ_FORMAT_CAPACITIES, SCSI_READ10, SCSI_MODE_SENSE6 and after device is detected in OS SCSI_TEST_UNIT_READY command is regular called. You can see my changes in usbd_storage_msd.c file attached. Best regards, John #stm32f2-usb-mass-storage2018-06-08 9:09 AM
I did not find a MSC SDRAM-DISK example for the STM32F429I-DISCO from 2015 anywhere.
Roman Marjamaa
Marjamaa Engineering Inc.
395 Co Rd 110 N
Mound, MN 55364
Direct: (612) 999-8263
Mobile: (612) 345-1492
Fax: (855) 627-5364
www.marjamaaengineering.com<http://www.marjamaaengineering.com/>;
All information contained in this email is to be treated as “confidential�? or “proprietary�? and shall not be shared
outside the terms of the Agreement between Marjamaa Engineering Inc. and the Recipients of this email.
2018-06-08 11:23 AM
https://community.st.com/0D50X00009XkgpRSAR
2018-06-08 11:55 AM
Thanks,
Roman Marjamaa
Marjamaa Engineering Inc.
395 Co Rd 110 N
Mound, MN 55364
Direct: (612) 999-8263
Mobile: (612) 345-1492
Fax: (855) 627-5364
www.marjamaaengineering.com<http://www.marjamaaengineering.com/>;
All information contained in this email is to be treated as “confidential�? or “proprietary�? and shall not be shared
outside the terms of the Agreement between Marjamaa Engineering Inc. and the Recipients of this email.
2018-12-03 5:49 AM
Hallo Clieve 2.0,
could you please repost this link to your example? Its broken again...
thanks a lot
2018-12-03 6:39 AM
Please have @brk dig it out of the archive of broken forums past..
It would have been F4 SPL code from 5 or more years ago.
2018-12-12 2:37 AM
2020-08-19 10:02 PM
@Community member I am using stm32f072rb discovery board... and I allocated 10 and tried also with 11kb ... It is showing 11kb in windows but error comes that widows is unable to format disk.. can you help me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.