2016-12-12 8:55 AM
hi everyone. i have 2 stm3241-g eval boards and i wanna establish communication between them by using usb protocol but i have no idea about usb. i have never used it. i need just communication like a rs232. i must use usb cause i need min 30Mb/s baud. i read some documents about protocol and i investigate example project. But this is not enough. especially usb class topic confusing me. Which class should i use etc. To sum up how can i transmit and receive raw data from mcu buffer to another mcu buffer by using usb ? thx
#usb #data-transfer2016-12-13 5:59 AM
Dear
ILTAR.Ismail_Fatih
,Are youusing a Cube example ? I think you can start with a working USB example within your associated STM32Cube firmware package where the workspace is ready to use. This will help you to have more idea on how configuration/implementation is done.
The STM32Cube USB device library UM1734 user manual will help youon how tousethe STM32Cube USB device library,which is applicable to all STM32 Series that feature an USB peripheral.
Best Regards
-Imen-
2016-12-13 6:56 AM
Evaluation board with STM32F417IG MCU .
So for understanding purposes, you have
Option 1- UM1734. No doubt somewhat correct but splattered with the effects of Translation, Interpretation, Comprehension, Business, Hollywood and Politics. For certain – NOT 100% believable.
Option 2 – README.TXT. Looks like it maybe came from the folks who were actually writing some of the code. When in doubt, believe the README FILE until proven wrong.
The code comments seem pretty spot on too.
If I were you, I'd hunt down the README.TXT file in the project workspace that is usually in a DOC folder and review that. So far - for the STM32L4 (CubeL4 Examples) anyway, It has proven much more accurate / clear than UM1734.
'but i have no idea about usb. i have never used it.'
Putting it mildly, you have a LOT to learn and I wish you good luck.
2016-12-13 9:45 AM
Thank you for all the comments
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.