2022-03-10 1:01 PM
My H7 board has a strange issue: if I connect it to USB, Windows recognizes it (PRODUCT ID & VENDOR ID are correctly shown) but no communication (by CDC_Transmit_FS()) happens: CDC_Transmit_FS reports me BUSY_USB.
If I reset (by the pushbutton) my board, all is OK, and the communication perfectly works!
After the "hard reset", I can unplug and replug my USB cable and the system works (of course, this is possible only if I use an external power supply).
Thanks and best regards
2022-03-10 10:14 PM
Seems on inserting your code hangs on an fault. Debug it ...
2022-03-10 11:14 PM
Unfortunately, it is not possible to access debugging functions: it is a custom board and I can program it by USB (there is a switch to set "Config Boot System" and to allow me USB programming by STMCubeProg), but STLink / JTAG /SWD Interfaces aren't accessible...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.