2016-02-10 1:49 AM
Hi,
I'm using the CDC class driver version 2.4.1 and made the following changes to the usbd_cdc_if.c template: Since the provided CDC_Transmit_FS function tries to transmit the packet forever, i.e.do {
result = USBD_CDC_TransmitPacket(hUsbDevice_0); } while(result != USBD_OK); this function blocks if the endpoint is not ready. Hence, I added a USB_Ready flag, which is set at the end of CDC_Init_FS and unset in CDC_DeInit_FS. In case the flag is unset, CDC_Transmit_FS returns immediately (with USBD_FAIL return code). Now I made a strange observation: I'm calling CDC_Transmit_FS from a high frequency loop. During the first iterations the transmit function fails, that's okay (I think). However, as soon as the ready flag is set, the first packet transmitted causes a call to CDC_Receive_FS with exactly the data I tried to send, while it actually never gets transmitted to the USB host. Therefore, I assume I try to send the data a bit too early. Does this makes sense to you? Is there a way to solve this problem? #stm32-usb-cdc-vcp2016-02-10 6:10 AM
I found the solution:
The CDC_Init_FS function was the wrong place to wait. Instead, one has to look for the CDC_SET_CONTROL_LINE_STATE command. It's just a pity that the wValue field of the USBD_SetupReqTypedef struct is not passed to the CDC_Control_FS function, since this tells you whether DTR (data terminal ready) is set or not. (Maybe an idea for the next release?)2017-05-22 10:00 AM
just add
bool CDC_IsConnected = ((USBD_HandleTypeDef*)hpcd_USB_OTG_FS.pData)->request.wValue & 0x01;
on the
CDC_SET_CONTROL_LINE_STATE switch path. should do it
2018-05-23 3:09 AM
Sorry for posting to old thread, but for others searching for a solution, this is what I did:
static int8_t CDC_Control_FS(uint8_t cmd, uint8_t* pbuf, uint16_t length)
{... case CDC_SET_CONTROL_LINE_STATE: { USBD_SetupReqTypedef * req = (USBD_SetupReqTypedef *)pbuf; if(req->wValue &0x0001 != 0) { // DTR is set... } }break;
...}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.