2023-11-26 12:58 PM - edited 2023-11-26 1:08 PM
I am currently working on a project in which my board is a lightweight version of a larger, more expensive unit. The other unit uses code where endpoint 0x81/0x02 are used for interrupt type. The endpoints for 0x83/0x04 are used for bulk USB. I only need to access bulk USB.
I have built the following device descriptor for my device:
/* USB MYDEV device Configuration Descriptor */
__ALIGN_BEGIN static uint8_t USBD_MYDEV_CfgDesc[USB_MYDEV_CONFIG_DESC_SIZ] __ALIGN_END =
{
0x09, /* bLength: Configuration Descriptor size */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType: Configuration */
USB_MYDEV_CONFIG_DESC_SIZ,
/* wTotalLength: Bytes returned */
0x00,
0x01, /*bNumInterfaces: 1 interface*/
0x01, /*bConfigurationValue: Configuration value*/
0x02, /*iConfiguration: Index of string descriptor describing the configuration*/
0x80, /*bmAttributes: bus powered and Supports Remote Wakeup */
0x32, /*MaxPower 100 mA: this current is used for detecting Vbus*/
/* 09 */
/********** Descriptor of MYDEV interface 0 Alternate setting 0 **************/
/*---------------------------------------------------------------------------*/
/* MYDEV Interface Descriptor */
0x09, /* bLength */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType */
0x00, /* bInterfaceNumber */
0x00, /* bAlternateSetting */
0x02, /* bNumEndpoints */
0xFF, /* bInterfaceClass: Vendor Specific*/
0xFF, /* bInterfaceSubClass: Vendor Specific */
0xFF, /* bInterfaceProtocol: Vendor Specific */
0x00, /* iInterface */
/*---------------------------------------------------------------------------*/
/*---------------------------------------------------------------------------*/
/* EP1 descriptor */
0x07, /* bLength */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType */
MYDEV_EPIN_ADDR, /* bEndpointAddress */
0x02, /* bmAttributes: bulk */
LOBYTE(MYDEV_EPIN_SIZE), /* wMaxPacketSize */
HIBYTE(MYDEV_EPIN_SIZE),
0x00, /* bInterval: */
/*---------------------------------------------------------------------------*/
/*---------------------------------------------------------------------------*/
/* EP2 descriptor */
0x07, /* bLength */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType */
MYDEV_EPOUT_ADDR, /* bEndpointAddress */
0x02, /* bmAttributes: bulk */
LOBYTE(MYDEV_EPOUT_SIZE), /* wMaxPacketSize */
HIBYTE(MYDEV_EPOUT_SIZE),
0x00, /* bInterval: */
};
#define MYDEV_CMD_PACKET_SIZE 64U
#define MYDEV_EPIN_ADDR 0x83U
#define MYDEV_EPIN_SIZE 64U
#define MYDEV_EPOUT_ADDR 0x04U
#define MYDEV_EPOUT_SIZE 64U
#define USB_MYDEV_CONFIG_DESC_SIZ 32U
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData, 0x00, PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData, 0x80, PCD_SNG_BUF, 0x58);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData, 0x83, PCD_DBL_BUF, 0x009800D8);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData, 0x04, PCD_DBL_BUF, 0x01180158);When I try to write data to endpoint 0x04 (host to device) I am getting I/O errors (using libusb)
When I change the endpoints to 0x81/0x02 and modify the application to use those endpoints I am able to send and receive data.
Is there something obvious I am missing with the device descriptor or misunderstanding of how endpoints are indexed?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.