2025-06-02 1:49 AM
Hello community,
I'm facing a UART communication issue with my STM32F042K6T6 board and would appreciate any insights. Here are the details:
Hardware Setup:
The Problem:
What I've Verified:
Signal Integrity:
Basic Tests:
NOTE : The stpm3x.h & stpm3x.c library is ported manually from CPP. I also attached the original CPP files for the reference.
2025-06-02 5:58 AM
> hal_status = HAL_UART_Receive(uart, recv, sizeof(recv), 1000);
> Loopback test (TX→RX) also not working properly as only the first byte is received others omitted.
You will need to use nonblocking functions to receive data as it comes in and store those into a buffer for use. There is no automatic handling of data beyond the single byte buffer--if two bytes get received and you haven't processed them yet, that will trigger an overflow, the peripheral will stop, and the data will be lost.
2025-06-02 6:02 AM
Hello @Muruganandam
Please refer to the UART example below:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.