2023-06-20 6:20 AM
Hi,
There is possible to set up USART2 on PA2 and PA15?
In documentation in both pins is possible to use USART2 (PA2 as TX and PA15 as RX).
I try do it, but I don't get interrupt when data is send to RX pin. On Uart1 (PA9, PA10) it's work correct.
For UART2 I used this same register configuration as for UART1.
//******************************
// Uart 1
//******************************
// clock enable
RCC->APBENR2 |= RCC_APBENR2_USART1EN;
USART1->BRR = (U16) (CLK_HCLK / DEF_HELP_RS_BAUD_RATE);
// DE Enable & Timing
USART1->CR3 |= USART_CR3_DEM;
USART1->CR1 |= USART_CR1_DEAT_0 | USART_CR1_DEAT_1 | USART_CR1_DEAT_2 | USART_CR1_DEAT_3 | USART_CR1_DEAT_4;
USART1->CR1 |= USART_CR1_DEDT_0 | USART_CR1_DEDT_1 | USART_CR1_DEDT_2 | USART_CR1_DEDT_3 | USART_CR1_DEDT_4;
// Configuration
// 8-bit length + no parity - nothing needn't be configured
// Enable interrupts: RxD
USART1->CR1 |= USART_CR1_RXNEIE_RXFNEIE;
// Enable: RxD | UART
USART1->CR1 |= USART_CR1_RE | USART_CR1_UE;
//******************************
// Uart 2
//******************************
// clock enable
RCC->APBENR1 |= RCC_APBENR1_USART2EN;
USART2->BRR = (U16) (CLK_HCLK / DEF_HELP_RS_BAUD_RATE);
// DE Enable & Timing
USART2->CR3 |= USART_CR3_DEM;
USART2->CR1 |= USART_CR1_DEAT_0 | USART_CR1_DEAT_1 | USART_CR1_DEAT_2 | USART_CR1_DEAT_3 | USART_CR1_DEAT_4;
USART2->CR1 |= USART_CR1_DEDT_0 | USART_CR1_DEDT_1 | USART_CR1_DEDT_2 | USART_CR1_DEDT_3 | USART_CR1_DEDT_4;
// Configuration
// 8-bit length + no parity - nothing needn't be configured
// Enable interrupts: RxD
USART2->CR1 |= USART_CR1_RXNEIE_RXFNEIE;
// Enable: RxD | UART
USART2->CR1 |= USART_CR1_RE | USART_CR1_UE;
2023-06-20 1:27 PM
Read out and check/post UART and relevant GPIO registers content.
> I don't get interrupt when data is send to RX pin.
Polled Rx works?
JW
2023-06-20 10:22 PM
I don't know why, but today when I started again testing communication, interrupts works correct.
So I don't know what was the problem, but for now is solved.
Anyway, Thanks for help :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.